[EXT_EP-11203] Using intrinsic __lookup_init causes INTERNAL ERROR on Windows Created: 20/Jun/23 Updated: 01/Apr/24 Resolved: 31/Jul/23 |
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
Internal ID: | CODEGEN-11224 |
Forum URL: | https://e2e.ti.com/e2eprivate/bosch/bosch---ti-automotive-processors/f/1223/t/1238207 |
Found In Release: | C6000_8.3.0 C7000_2.1.0.LTS C7000_3.1.0.LTS |
Fix In Release: | C7000_2.1.3.LTS* C7000_3.1.1.LTS C6000_8.3.13 C7000_4.0.0.STS |
Affected Platform/Device: | default |
Description |
The attached test case has these lines ... // COMMENT OUT THIS LINE AND IT BUILDS CLEAN __lookup_init(__LUT_SET0, __as_uint16(value_to_set), (uint32_t)(i)); Build it ... % cl7x -@options.txt example.cpp INTERNAL ERROR: cg7x experienced a segmentation fault while processing function _Z17init_lut_example1v This is caused by a defect in the TI G3 C/C++ Codegen. TI Customer Support may be able to suggest a workaround to avoid this. Upgrading to the newest version of the compiler may fix this problem. Contact TI in the E2E support forums at http://e2e.ti.com under "Development Tools", "TI C/C++ Compiler". See the link titled "Submitting an issue". We need to see this ENTIRE error message and a complete, reproducible test case including ALL of the command-line options. Include the .pp file created by option --preproc_with_comment >> Compilation failure |