[EXT_EP-10888] Document '#pragma clang section bss' to be used for uninitialized variables Created: 29/Aug/22  Updated: 12/Sep/22  Resolved: 12/Sep/22
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
Internal ID: CODEGEN-10383
Forum URL: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1129204/tda4vm-tiarmclang-compiler-issue-only-the-first-clang-data-section-in-a-c-file-was-retained-after-compiled-as-an-object-file-others-are-missing
Found In Release: ARMCLANG_2.1.1.LTS
ARMCLANG_1.3.0.LTS
Fix In Release: ARMCLANG_2.1.1.LTS
ARMCLANG_1.3.2.LTS*
Affected Platform/Device: default

 Description   

The attached source file has these lines ...

#pragma clang section data="one_data"
static volatile uint32_t var1 = (uint32_t)(0U);
#pragma clang section data=""

#pragma clang section data="two_data"
static struct sss_tag sss_instance;
#pragma clang section data=""

Build it ...

% tiarmclang -S file.c

Inspect the resulting file.s. Both variables get created. The first one is created in the user-named section. The second one is created in the default section .bss, and not the user-named section.


Generated at Wed Apr 23 06:33:36 CDT 2025 using Jira 9.12.17#9120017-sha1:aba4002bcd633f188b6a4bb5dd8a0e1f20b79ee4.