[EXT_EP-10834] LTO: linker should include undefined symbols that are referenced from a static function in the IR symbol table that is passed to the LTO recompile Created: 09/Jun/22 Updated: 06/Sep/22 Resolved: 06/Sep/22 |
|
Status: | Fixed |
Project: | Embedded Software & Tools |
Component/s: | None |
Affects Version/s: | None |
Fix Version/s: | None |
Type: | Bug | Priority: | High |
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
Internal ID: | CODEGEN-10067 |
Found In Release: | ARMCLANG_2.1.1.LTS |
Fix In Release: | ARMCLANG_2.1.1.LTS |
Affected Platform/Device: | default |
Workaround: | This issue should not arise when using the 2.1.0.LTS (or later) version of the TI Arm Clang Compiler Tools since a fix to a related issue https://sir.ext.ti.com/jira/browse/EXT_EP-10829 will prevent the linker from failing due to this issue. |
Description |
An externally defined symbol that is referenced from a static function or variable whose section is included in the reference graph should be included in the intermediate representation's symbol table that is presented to the link-time optimizer for recompilation. For example, if t1.c contains a static function definition that references RTS functions expf and logf and the address of the static function is made available in a data object that is externally accessible, then the expf and logf symbols should be recognized and included in t1.o's intermediate representation module as legitimate unresolved symbol references. |