[EXT_EP-10175] Hex utility, when splitting a section as required by the bootloader, ignores the section alignment for the second part of the split Created: 28/Dec/20  Updated: 13/Oct/25  Resolved: 20/Apr/22
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
Product: Code Generation Tools
Internal ID: CODEGEN-8471
Forum URL: https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/964813
Found In Release: C2000_21.12.0.STS
ARMCLANG_2.1.0.BETA1
ARM_18.12.0.LTS
ARMCLANG_1.3.0.LTS
C2000_21.6.0.LTS
ARM_20.2.0.LTS
C2000_20.2.0.LTS
Fix In Release: ARM_20.2.7.LTS
ARMCLANG_2.1.1.LTS
C2000_22.6.0.LTS
C2000_20.2.7.LTS
ARMCLANG_1.3.2.LTS*
ARM_18.12.9.LTS*
C2000_21.6.1.LTS
Affected Platform/Device: default
Workaround: Determine which sections exceed the length limit of 0xfffe words. Then apply LINKER command file section splitting to those sections so the hex utility does not see a section longer than 0xfffe words. For an example, see https://e2e.ti.com/support/microcontrollers/c2000/f/171/p/964813/3571661#3571661

 Description   

The option --boot tells the hex utility all the initialized sections are to be laid out as required by the on-chip bootloader.  This bootloader cannot handle any section which is larger than 0xfffe words.  So, when this occurs, the hex utility splits the section up, and starts another bootload-style record for the next part of the split.  When this happens, the hex utility fails to check the alignment requirements of the section to make sure the the starting address of the second record meets that alignment.  


Generated at Sat Dec 13 11:34:41 CST 2025 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.