[EXT_EP-10085] Code coverage symbols not defined when profile counter section manually placed Created: 22/Oct/20  Updated: 30/Nov/22  Resolved: 30/Nov/22
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
Internal ID: CODEGEN-8216
Found In Release: ARMCLANG_2.1.0.LTS
ARMCLANG_1.3.0.LTS
ARMCLANG_2.1.2.LTS
Fix In Release: ARMCLANG_1.3.2.LTS*
ARMCLANG_2.1.3.LTS*
Affected Platform/Device: default
Workaround: The workaround is that the client either shouldn’t explicitly place the section, or if it does, the symbols should also be explicitly defined based on the section location.  If users don't explicitly place the section, the linker will place it based on the location of the .bss section.

 Description   

In looking at the linker, it appears that if the _llvm_prf_cnts section is explicitly placed by the linker command file, then the “start_llvm_prf_cnts" and "stop__llvm_prf_cnts" symbols are not created. 
The workaround is that the client either shouldn’t explicitly place the section, or if it does, the symbols should also be explicitly defined based on the section location.  If users don't explicitly place the section, the linker will place it based on the location of the .bss section.


Generated at Thu Apr 03 04:42:52 CDT 2025 using Jira 9.12.17#9120017-sha1:aba4002bcd633f188b6a4bb5dd8a0e1f20b79ee4.