Export - CSV (All fields)
Export - CSV (Current fields)
EXT_EP-7591
pow(2,x) has fairly significant rounding errorEXT_EP-7705
DWARF does not correctly represent variables stored in register pairsEXT_EP-7722
Extern inline functions are not supported in the C/C++ Compiler with COFF ABIEXT_EP-7757
C2000 can't print 0 with %a formatEXT_EP-7763
strcmp doesn't correctly handle values with uppermost bit setEXT_EP-7767
hex2000, while using -b option, mistakenly states a section "falls in unconfigured memory"EXT_EP-7800
Forward reference in .space generates an internal errorEXT_EP-7829
printf gives wrong value for pointer when its value is incrementedEXT_EP-7897
C2000 RTS float arithmetic functions do not round correctlyEXT_EP-7954
C2000 float software multiply doesn't handle -1*INF properlyEXT_EP-8006
Linker gives misleading warning when dot expressions used in SECTION directive for .stack sectionEXT_EP-8023
Structure is not initialized correctly when using -o2 or -o3 optimizationEXT_EP-8550
error with using constexpr for return from end() with empty std::initializer_listEXT_EP-8551
wostringstream::fill(WCHAR_MAX) incorrectly sets the fill value to ' 'L.EXT_EP-8580
libcxx/include/random uses unsigned for unsigned longEXT_EP-8582
noexcept(typeid(d)) runtime fail on polymorphic class typeEXT_EP-8583
deeply nested lambda functions causes a hang in the code generatorEXT_EP-8585
No error generated for lambda-expression in default argument cannot capture any entity.EXT_EP-8589
<regex> never throws error_ctypeEXT_EP-8712
Unimplemented core issue 1769: Catching a thrown derived class by reference to base clasEXT_EP-8720
cannot find matching "==" operator definitionEXT_EP-8727
Composing operations for valarray may fail to compileEXT_EP-8730
Exception propagating out of noexcept function does not call std::terminateEXT_EP-8731
std::linear_congruential_engine doesn't support 8-bit resultsEXT_EP-8733
libcxx istreambuf_iterator points to end of string instead of character past matchEXT_EP-8737
Multiple non-variables may be declared using auto or decltype(auto)EXT_EP-8745
cerr.tie() returns the wrong valueEXT_EP-8749
1 ULP rounding error in double additionEXT_EP-8752
Compiler aborts with excessive inlining of C++ functionsEXT_EP-8756
Internal error when passing a temporary array of objectsEXT_EP-8757
Cannot take the address of std::ctype<char>::table_sizeEXT_EP-8759
wstring runtime failure - likely bug in swprintfEXT_EP-8760
Unexpected type returned by bitset [] operatorEXT_EP-8762
std::multimap::clear is not noexceptEXT_EP-8766
regex_constants::ECMAScript not expected to be 0EXT_EP-8767
armcl allows non-default arguments to be specified after default argumentsEXT_EP-8768
Internal error when assigning default arguments to a parameter packEXT_EP-8770
Failure to defer C++ access control checksEXT_EP-8771
decltype cannot be used as a destructor nameEXT_EP-8772
Unimplemented core issue 475: std::uncaught_exception is not true when constructing the thrown objectEXT_EP-8826
std::num_get does not parse floating-point strings correctlyEXT_EP-8990
Using --gen_profile_info with code with CLA source fails to buildEXT_EP-8993
Typo on ULP Advisor messageEXT_EP-9004
Simple syntax error causes assembler to fail with INTERNAL ERROREXT_EP-9037
When a symbol is remapped, DW_TAG_TI_branch/DW_AT_name is not updatedEXT_EP-9306
Erroneous "redeclared with incompatible type" involving two tagless structs with same formEXT_EP-9433
Compiler error: no instance of function template matches the argument listEXT_EP-9771
The option --preproc_dependency mishandles spaces in directory namesEXT_EP-10056
Rounding error in floating point division of constant valuesEXT_EP-10116
C++ header files do not build clean with --issue remarks
{"errorMessages":["jqlTooComplex"],"errors":{}}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0