Export - CSV (All fields)
Export - CSV (Current fields)
- EXT_EP-8432
TIRex fails to open when installing CCS for Linux as sudo but running as user - EXT_EP-9754
Resource Explorer should place temporary file in standard location - EXT_EP-8964
Variables/Expressions view displays incorrect values for virtual inheritance example - EXT_EP-9576
CCS: Extreme flickering when resizing panel that shows Getting Started, SysConfig or Resource Explorer - EXT_EP-9563
CCS IDE flickers on mouse movement when ROV and ReX is opened on Linux - EXT_EP-9300
[CDT] Creating and building a new build configuration of mmWave example project results in build error - EXT_EP-9009
Macro expansion shown in the IDE does not match with how the compiler expands the macro - EXT_EP-10026
Resize cursor does not show up after browser based windows are open - EXT_EP-9550
CCS editor assumes the macro __cplusplus is always defined even when it is not - EXT_EP-9603
Editor highlighting of conditional statements based on the __cplusplus symbol is incorrect - EXT_EP-9525
.TI.noinit and .TI.persistent should be treated specially when verifying a program - EXT_EP-10212
Getting started view has a vulnerability to remote execution with man-in-the-middle attack - EXT_EP-10035
CCS 10.x missing Windows registry entry which specifies the version number - EXT_EP-9799
Scripting Console: Commands like "cleanProject" timeout for GIT projects when GIT label decorations are enabled - EXT_EP-9800
Hex output format should not allow selecting --array or --binary as standalone options - EXT_EP-9827
CCS 10.0 does not check correct endianess when loading a program - EXT_EP-9744
UART pin config lost when flow control enabled - EXT_EP-9678
(Linux) Any attempt to remove a single search path removes all entries - EXT_EP-9770
Using context menu to manage versions does not update the package version list - EXT_EP-9655
Importing mmWave project via Resource Explorer results in incorrect device setting - EXT_EP-9759
Link from Project Wizard to Resource Explorer does not work - EXT_EP-9732
Building SysConfig projects fail if installation directory has spaces - EXT_EP-9731
Running "dss" (with no parameters) prints out cryptic error message - EXT_EP-9748
CCSv10.0.0 Splash Screen says v9 on macOS - EXT_EP-9614
CCS crashes when attempting to restore a breakpoint with a register trigger type not supported on the device - EXT_EP-9730
Start menu shortcuts are missing version on Windows 10 - EXT_EP-9751
CCSv10 does not startup after downloading a compiler update - EXT_EP-8174
TIRex search bar disappears depending on the viewport size - EXT_EP-8435
Duplicate "Software" node appears when downloading SimpleLink SDK - EXT_EP-9601
SDK installation using CCS REX results in some utilities being in incorrect format
{"errorMessages":["jqlTooComplex"],"errors":{}}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0