Export - CSV (All fields)
Export - CSV (Current fields)
- EXT_EP-9743
Compiler incorrectly issues remark: value copied to temporary, reference to temporary used - EXT_EP-10220
Compiler mistakenly includes user header file instead of system one - EXT_EP-10347
Generated coverage .csv file has duplicate entries - EXT_EP-10484
Add diagnostic if more than one --global_register option is supplied - EXT_EP-10950
Compiler inconsistently handles multiple definitions of a global variable in different files with and without link time optimization - EXT_EP-11071
TI proprietary assembler incorrectly rejects add instruction that refers to the PC - EXT_EP-11012
Compiler generates incorrect code for 64-bit comparison against small constant, when --opt_level=3 or higher - EXT_EP-11103
_Pragma("diag_suppress 179") has no effect when used inside a macro, but works when used outside a macro - EXT_EP-11551
armobjcopy fails with error: invalid alignment 1 of group section - EXT_EP-10156
Incorrect handling of floating point constant -0.0 - EXT_EP-10637
Incorrect initialization of implicitly-sized array from constant initialization value with designated initializers - EXT_EP-8606
std::rethrow_if_nested does not have standard signature - EXT_EP-8605
operator<<(std::basic_ostream<K,T>&, const std::error_code&) is not defined in system_error - EXT_EP-8603
scoped_allocator_adaptor can't be explicitly instantiated with two arguments - EXT_EP-8608
C++ header file cuchar is not provided in libc++ - EXT_EP-8596
Access of const static member through pointer is not a constant expression. - EXT_EP-8599
std::reference_wrapper doesn't define argument_type for classes containing a typedef member named argument_type - EXT_EP-8590
std::function<T>::target_type() should return typeid(void) if target is empty - EXT_EP-8725
cannot find definition of ">=" operator - EXT_EP-8716
Parser errors on empty enum declaration - EXT_EP-8711
Incomplete class type when using various members of <iterator> - EXT_EP-8607
nested_exception::rethrow_nested() not supported - EXT_EP-8591
shared_ptr::get_deleter() should return the original deleter class without copying - EXT_EP-8602
Problem with std::swap and <tuple> - EXT_EP-8597
No diagnostic issued if an allocation function throws a non bad_alloc exception - EXT_EP-8604
Raw string d-char-sequence isn't supported - EXT_EP-8740
armcl fails to flag an inconsistent use of alignas between a declaration and definition of an object - EXT_EP-8738
armcl errors on legal constexpr constructor call - EXT_EP-8769
armcl allows illegal attribute in friend declarations - EXT_EP-8593
wofstream << operator unexpected termination with wchar_t - EXT_EP-8115
#pragma LOCATION and palign do not work together - EXT_EP-8118
Automatic library build fails when an exact library name is used - EXT_EP-7639
Compiler does not respect partial overrides in C99 designated initializers - EXT_EP-7603
Should allow "ADD R0, R1, #0xfff" for v6m0 - EXT_EP-7807
Should accept 2-operand SUB SP in Thumb1/UAL mode - EXT_EP-8045
Missing __aeabi_read_tp - EXT_EP-7844
Missing half-precision float conversion functions - EXT_EP-8114
The armhex command does not handle spaces in the name of the output binary - EXT_EP-7777
Complex math - when the imaginary part of z is infinity, cprojf(z) is computed incorrectly - EXT_EP-7928
Should accept "LDRD R8,[R1]" in Thumb-2 mode - EXT_EP-7676
Missing AEABI_COMPATIBILITY_MODE link-time constants - EXT_EP-8064
Assembler accepts but mistranslates BLLT in v7 thumb mode - EXT_EP-7836
Disable diagnostic 1558 (--float_operations_allowed diagnostic) in standard header files - EXT_EP-8766
regex_constants::ECMAScript not expected to be 0 - EXT_EP-7964
Cortex-M0 library lacks uread4, etc. - EXT_EP-7805
The _ssat16 intrinsic allows literals in the range of 0-31, but the SSAT16 instruction only accepts values from 1-16 - EXT_EP-7759
The .label assembler directive should not be accepted when assembling for ELF. - EXT_EP-9004
Simple syntax error causes assembler to fail with INTERNAL ERROR - EXT_EP-8759
wstring runtime failure - likely bug in swprintf - EXT_EP-7848
ARM assembler does not issue a warning for PC-relative loads when --embedded_constants=off
{"errorMessages":["jqlTooComplex"],"errors":{}}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0