Export - CSV (All fields)
Export - CSV (Current fields)
EXT_EP-9612
CCS shows wrong C7x assembly decoding of instruction machine codeEXT_EP-9836
Disassembler may not show sign extension of immediate valuesEXT_EP-9841
__vstore_reverse_bit variants reverse output of complex types in big endianEXT_EP-9847
__store_predicate_char intrinsic gives incorrect result in big endianEXT_EP-10279
Documentation and linker diagnostics do not cover dependency between .cinit and GROUP placementEXT_EP-11874
assignment to a bit field mistakenly overwrites entire bit field structureEXT_EP-11907
Improve compiler documentation for -ftEXT_EP-11966
lambda function near cfloat8 *= cfloat8 causes internal errorEXT_EP-12184
symbol table entry for the compiled file should indicate source file name but instead has either a temp file name or the file's assembly file nameEXT_EP-12752
The compiler returns a successful exit code to the OS despite missing cmd options fileEXT_EP-12793
Compiler fails with INTERNAL ERROR: opt2000 experienced a segmentation faultEXT_EP-12901
Improve compiler documentation for -ftEXT_EP-12907
Dwarf call frame information contains frame description entries with instructions with the wrong addressEXT_EP-12936
C7000 Host Emulation SE load of scalar floating point has incorrect valueEXT_EP-12967
Missing dependency edge due to incorrect alias disambiguationEXT_EP-13038
Under some conditions, including use of --opt_level=2, C++ code that throws an exception runs awayEXT_EP-13061
parser converts gnu statement expressions in for loops to incorrect loop increment that occurs too early in loop codeEXT_EP-13150
Linker crashes while processing local common symbolsEXT_EP-13151
Write to a volatile vector may be discardedEXT_EP-13190
Use of lambda causes C7x host emulation to produce different results than normal C7x executionEXT_EP-13232
Using --opt_level=0 with intrinsics like __complex_multiply generates incorrect code
{"errorMessages":["jqlTooComplex"],"errors":{}}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0