Export - CSV (All fields)
Export - CSV (Current fields)
- EXT_EP-11476
Conditional watchpoint is ignoring condition and always triggers - EXT_EP-11552
XDS110 USB enumeration and autodetect issues with split launchpads - EXT_EP-11598
CCS is not halting at the __mdebugstop() directive on a F28P65x device - EXT_EP-9480
EnergyTrace HDR fails to run past one minute or two on macOS - EXT_EP-10557
ET/ET++ does not work during a debug session on CC1310 - EXT_EP-9918
Improve error message when EnergyTrace is launched on an unsupported device - EXT_EP-10918
TVT: Unable to open up TDF file if the symbol file has been moved/renamed - EXT_EP-11167
TVT: Code Profile/Coverage view - Unable to expand file name to see Function and Line data - EXT_EP-11023
XDS110: Unable to flash boot_loader.bin on Linux - EXT_EP-10920
TVT: Function/File/Directory information for some entries missing when opening TDF file in Trace viewer - EXT_EP-9143
Port stune to Linux and macOS - EXT_EP-10916
TVT Linux: Can only save collected trace data as a TDF file - EXT_EP-10917
TVT Linux: Trace data imported from a TDF file can only be saved as a sqlite file - EXT_EP-10244
CCS crashes when HW trace is enabled (via ETB) on the C674x of an IWR6843ISK - EXT_EP-10675
TVT: CCS Linux crashes when running target after Variable profiling is enabled - EXT_EP-10639
AWR294 Pin trace not currently supported. Buffer trace (ETB) supported - EXT_EP-10245
TVT: Core Trace doesn't support 64-bit addresses as trigger address - EXT_EP-10530
Core trace invoking the wrong instance on second invocation on a different instance of a core - EXT_EP-10237
AM64x: Cortex-M4 Core Trace: TDF file is saved incorrectly - EXT_EP-10336
"Erase and download necessary segments only" flash option still erases part of flash that it should not - EXT_EP-10249
macOS Big Sur: not able to move around views - EXT_EP-10353
CCS hangs on launch when git projects are imported to the workspace and the host computer is rebooted - EXT_EP-10267
Flash programming error message when connecting to a device without flash - EXT_EP-10221
"MSP430: Error connecting to the target: Unknown device" on Linux - EXT_EP-10240
Issue with demangling name from enum member - EXT_EP-10228
SysConfig in Cloud "Failed to save changes" error - EXT_EP-9486
Trace should automatically bypass the MMU / MPAX
{"errorMessages":["jqlTooComplex"],"errors":{}}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0