Export - CSV (All fields)
Export - CSV (Current fields)
EXT_EP-10367
math.h does not work with -std=c89 or c90 or gnu90EXT_EP-10632
Use of -save-temps causes warning diagnostic to not be emittedEXT_EP-10877
tiarmclang mishandles debug directives in TI-syntax assembly filesEXT_EP-10943
Debugger is unable to step in to an assembly macro in an include fileEXT_EP-11738
The instructions DMB and NOP are disassembled incorrectly by tiarmdisEXT_EP-11749
tiarmclang linker emits inadvertent but harmless warning when LTO is enabledEXT_EP-11784
tiarmclang constructs an invocation of the linker that exceeds the command line length supported by WindowsEXT_EP-11791
Linker command file with very long line causes tiarmclang to fail with fatal error: source line too longEXT_EP-11947
Code coverage instrumented files fail to assemble when -save-temps or -S is usedEXT_EP-12044
Compiler inconsistently emits diagnostic "argument unused during compilation" when C file isn't providedEXT_EP-12196
Building with LTO results in two 16-bit thumb NOP instructions to be issued in 32-bit Arm modeEXT_EP-12203
Compiler and documentation disagree on whether ACLE intrinsic __fmaf is supportedEXT_EP-12626
Documentation is missing for tiarmclang -mmathacl optionEXT_EP-12758
Use of -Og generates code that is hard to debugEXT_EP-12933
Compiler documentation incorrectly states bit fields are limited to a width of 32-bits. The correct limit is 64-bits.EXT_EP-12958
CMake definition of CMAKE_ASM_COMPILE_OBJECT puts the flags after the source file, which makes it impossible to add -x ti-asmEXT_EP-13005
Use of LTO causes linker to fail due to multiple definitions of compiler RTS functionsEXT_EP-13228
In some circumstances, assignments to fields in a local structure are ignoredEXT_EP-13252
tiarmclang: with LTO and FPU enabled, linker will generate a target triple incompatibility warning on divdf3_fast and muldf3_fastEXT_EP-13383
QKIT: setting COVFILELIST in CCS IDE for coverage compare needs workaround
{"errorMessages":["jqlTooComplex"],"errors":{}}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0